The Vishay Advantage: Robust Solutions for Extreme Industrial Environments
From fast chargers to energy management systems and motor drives, applications in industrial settings can expose components to extreme temperatures, moisture, dust, and corrosive substances. Therefore, engineers must design solutions that are durable and can withstand these conditions without compromising performance. Partnering with Vishay — a global leader in discrete semiconductors and passive electronic components — ensures access to advanced technology and reliable components for robust, durable, and efficient industrial end products. Vishay’s expansive portfolio streamlines the design process, enabling access to a breadth of essential components. This not only guarantees consistency in quality but may also result in reduced time to production. For those seeking to elevate their industrial designs to the next level, explore Vishay’s design solutions and featured components.
- Energy Storage
- Motor Drive
- DC Fast Charging
VOM1271 Photovoltaic MOSFET Driver
Unlike conventional MOSFET drivers, which require an external power supply to provide VCC and or VDD rails to the driver itself, the VOM1271 obtains all the required current to drive its internal circuitry from the LED current on the low voltage primary side of the isolation barrier.
RAMK060 Magnetic Encoder
RAMK magnetic encoders offer high resolution, high accuracy, high precision and optional multi-turn function in packages ranging from 27mm to 90mm in diameter. Magnetic encoders are execellent for industrial applications as they are impervious to humidty and dust in the operating environment.
VOM1271 Photovoltaic MOSFET Driver
Unlike conventional MOSFET drivers, which require an external power supply to provide VCC and or VDD rails to the driver itself, the VOM1271 obtains all the required current to drive its internal circuitry from the LED current on the low voltage primary side of the isolation barrier.