• Preferred Supplier

Melexis

Image of Melexis IMC Technology

Lateral Sensing with IMC Technology

As many traditional Hall Effect sensors are only sensitive to magnetic flux perpendicular to the IC, it can be necessary to develop complex (and therefore large and expensive) custom magnetic structures to achieve the desired measurement. Melexis’ latch & switch sensors use the innovative magnetic Triaxis® technology that allows the measurement of the lateral magnetic flux component.

Image of Melexis Triaxis MLX90380

Second-generation Triaxis Resolver Motor Position Sensor MLX90380

The MLX90380 is a fast pre-programmed magnetic resolver IC for brushless motors. It is ideally suited to automotive applications as well as other applications that need fast position readouts.

Image of Melexis Intelligent Approach to Eliminating Thermal Disturbances

An Intelligent Approach to Eliminating Thermal Disturbances in Non-contact Temperature Measurement

As we become more conscious of our health and our environment, temperature sensing is becoming increasingly relevant. As a result, it is a function now being added to many devices, including health monitoring devices in the form of medical body thermometers and smart wearable devices.

Esittelyssä olevat videot

Melexis MLX90397 3D Magnetometer | Datasheet Preview
Melexis MLX90397 3D Magnetometer | Datasheet Preview
3D Magnetic Field Sensor IC (Magnetometer)
3D Magnetic Field Sensor IC (Magnetometer)
MLX90632 Surface Mount Medical Grade version temp sensor
MLX90632 Surface Mount Medical Grade version temp sensor
MLX90632 Medical Grade surface mount FIR (Far InFrared) Temp Sensor
MLX90632 Medical Grade surface mount FIR (Far InFrared) Temp Sensor
Näytä kaikki

Tietoja yrityksestä Melexis

Combining a passion for technology with truly inspired engineering, Melexis designs, develops and delivers innovative micro-electronic solutions that enable designers to turn ideas into applications that support the best imaginable future. The company’s advanced mixed-signal semiconductor sensor and actuator components address the challenges of integrating sensing, driving and communication into next-generation products and systems that improve safety, raise efficiency, support sustainability and enhance comfort.

Melexis is headquartered in Belgium and employs over 1,500 people in 19 locations worldwide. The company is publicly traded on Euronext Brussels (MELE).