At higher voltages the capacitance retention is still more than 90% at –55°C and 120Hz but there is more fall off at higher frequencies. Notice however that the 5% capacitance retention at 10kHz is 50µF - a lot of capacitance.
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
At higher voltages the capacitance retention is still more than 90% at –55°C and 120Hz but there is more fall off at higher frequencies. Notice however that the 5% capacitance retention at 10kHz is 50µF - a lot of capacitance.
Kiitos!
Seuraa sähköpostiasi, saat uutisia ja päivityksiä DigiKeyltä.
Syötä sähköpostiosoite
Hyväksy valintaruutu