A nice feature of the .11 family is to be able to update the firmware as necessary while the module is in the product out in the field. There is a single firmware update command that does a single http get from the host remote server.
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
A nice feature of the .11 family is to be able to update the firmware as necessary while the module is in the product out in the field. There is a single firmware update command that does a single http get from the host remote server.
Kiitos!
Seuraa sähköpostiasi, saat uutisia ja päivityksiä DigiKeyltä.
Syötä sähköpostiosoite
Hyväksy valintaruutu