Dynamic testing means that the electronic load can be switched between two set parameters according to the set rules. IT8500G+’s dynamic mode could test up to 20kHz. This function is used to test the dynamic characteristics of power supplies.
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
Dynamic testing means that the electronic load can be switched between two set parameters according to the set rules. IT8500G+’s dynamic mode could test up to 20kHz. This function is used to test the dynamic characteristics of power supplies.
Kiitos!
Seuraa sähköpostiasi, saat uutisia ja päivityksiä DigiKeyltä.
Syötä sähköpostiosoite
Hyväksy valintaruutu