An expensive liquid crystal display is not necessary for displaying data in most applications instead a seven-segment display is simply sufficient.
In this project, you will be building an object detection DC motor controller.
In this teardown, we will look at a windup radio with a few interesting features that may be useful in the wild!
You can connect Arduino sensors, actuators, and other ICs with the digital inputs and outputs (digital I/O) on the Arduino for useful things, such as reading switch inputs, lighting indicators, and controlling relay outputs.
It's easy to make a digital voltmeter with an Arduino and a 16x2 liquid crystal display (LCD). This project will also help you measure voltages above the reference voltage using a voltage divider.
Raspberry Pi is a miniature computer with ports that can be connected to different peripheral devices. It has an HDMI port to connect a monitor, USB ports for a keyboard and mouse, and an Ethernet port to connect to the internet.
Kiitos!
Seuraa sähköpostiasi, saat uutisia ja päivityksiä DigiKeyltä.
Syötä sähköpostiosoite
Hyväksy valintaruutu