In this blog we will explore the general design that can be used to create a wireless two player game, like Run Along, Jump & Jump. We will start with the basic game design, focusing on how the core game functionality works in both single player and two player versions.
Board game nerds rejoice! This beautifully simple laser cut project uses only one material and is an extremely buildable and customisable project that is easy to add your own style to.
Building a project from the ground up can be intimidating, especially when designing around an existing electroni
This vanity mirror incorporates some easy soldering and uses some of our special finish Value Acrylics. Once plugged into a USB wall plug, the LEDs inside will light up the viewer for optimal makeup application, beard trimming and silly-face-making. Read on to find out how you can make it!
This project is a brilliant base for further customisation. Change the designs on the walls, scale it, make a bracket to affix it to a wall, or a loop to hang it from a tree.
This Pedestrian Crossing project was submitted to us by Thomas Stratford. Thomas started this project to try out the pre-written code that came with the IET Pedestrian Crossing resource. The aim is to use the BBC micro:bit to develop a prototype for a pedestrian crossing for a local secondary school.
If you want to learn to code, learning to write games is a great way to get started, and our new hand held gamer has everything you need right now and it also has the connectivity for everything you might need tomorrow.
Introducing the new ARCADE Max for Makecode Arcade from Kitronik, gamification has never been this exciting! It’s our smallest handheld gamer to date but packs the biggest screen we’ve ever had!
For the budding Roboteer, learning how to add and control actuators is a key skill. In this guide, we are going to take a look at our servo driven Klaw actuator,* and show you how to control it via code.
CreateAI for BBC micro:bit brings AI to life through movement and play, perfect for curious young minds.
Mirrors are a great maker project to undertake because of their versatility in design and the fascinating history they carry.
This is a step by step guide for using free design tools to create 2D and 3D designs for 3D printing and is intended as an introduction to 3D design.
In this guide we are going to look at how you can use the package manager in Thonny to download the libraries for Kitronik products directly onto your Raspberry Pi Pico.
In this tutorial we’ll demonstrate how a Raspberry Pi Pico can be used along with some simple electronic components and Python code to record the voltage of a AA battery.
Kiitos!
Seuraa sähköpostiasi, saat uutisia ja päivityksiä DigiKeyltä.
Syötä sähköpostiosoite
Hyväksy valintaruutu