VideoLibrary

STM32WB5MM-DK Discovery Kit - Unboxing | DigiKey

Inside you’ll find the STM32WB5MM-DK board which integrates the FCC pre-certified, low power 2.4GHz STM32WB5MMG Module with diverse MEMS sensors, Quad-SPI flash, RGB display, microphone, multiple LEDs and buttons, STLink/V2 debugger, and flexible power supply options.

https://www.digikey.com/en/product-highlight/s/stmicroelectronics/stm32wb5mm-dk-discovery-kit

Features include 1 megabyte flash memory and an RF transceiver with numerous wireless projects in the STM32Cube.WB FW Library that supports BLE, BLE MESH, Zigbee, Thread, Matter, and proprietary protocols. The STM32Cube ecosystem includes a UI for configuration and initialization code generation, RF testing, a programmer for installing and upgrading protocol stacks, and free Eclipse-based STM32CubeIDE.

This Discovery Kit ships with pre-flashed firmware so that users can turn it on and immediately explore its capabilities.

First, download the ST BLE sensor app on your mobile device with Bluetooth active. Using the ST link micro USB port, connect the Discovery Kit to your computer and open the STM32 Cube IDE. Login to your myST account, and then click “Start New STM32 Project.” Under the Example Selector tab, use the “board filter” option to select the STM32WB5MM-DK board. In the “Examples List,” select BLE_HeartRate, and click next. Click finish once the example setup is complete. Now click the debug tool, and run the BLE_HeartRate example.

The Discovery Kit can now monitor heart-rate from the mobile app, using the BLE connection.

Learn more: Maker.io - https://www.digikey.com/en/maker DigiKey’s Blog – TheCircuit https://www.digikey.com/en/blog Connect with DigiKey on Facebook https://www.facebook.com/digikey.electronics/ And follow us on X (Formerly Known as Twitter) https://twitter.com/digikey

00:00 Intro 00:30 Features 01:09 STM32 Cube 01:44 Demo 02:41 Outro

7/30/2024 1:33:08 PM

Part List

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
DISCOVERY KIT WITH STM32WB5MMG MSTM32WB5MM-DKDISCOVERY KIT WITH STM32WB5MMG M20 - Immediate$73.94Näytä tiedot