VideoLibrary

STM32MP1 Primer – Day 4

This is Day 4 of our lecture series and thus far the stars of the show have been OpenSTLinux and the Cortex-A7. Wait a minute. We have access to a Cortex-M4 capable of running in excess of 200 MHz. With that today's discussion will focus on loading up the Cortex-M4 with a TOF (Time of Flight) application. We'll start the project from scratch and take a look at what it takes to configure our Cortex-M4 using the same STM32CubeMX and STM32CubeIDE environment we have been using all week. The Cortex-M4 that is native to the STM32MP157x hardware does not have access to standard flash program memory. Instead, we have 448K of embedded SRAM that we can fill with our Cortex-M4 application code. Despite the talents possessed by the Cortex-M4we still need OpenSTLinux to assist us in getting the Cortex-M4 code loaded and kicked off. Since OpenSTLinux must be running anyway along the way we'll see if we can offload any of the TOF application tasks to the Cortex-A7. The STM32MP157x-DKx discovery boards are fitted with an Arduino pin set on the bottom side of the board. This is a great time to introduce some home brewed Arduino-click-STM32MP1 interface hardware.

1/29/2025 8:43:23 PM

Microprocessors

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
IC MPU STM32MP1 800MHZ 361TFBGASTM32MP157FAC1IC MPU STM32MP1 800MHZ 361TFBGA2411 - Immediate$14.58Näytä tiedot
IC MPU STM32MP1 650MHZ 448LFBGASTM32MP157CAA3IC MPU STM32MP1 650MHZ 448LFBGA199 - Immediate$15.27Näytä tiedot
IC MPU STM32MP1 650MHZ 448LFBGASTM32MP151CAA3IC MPU STM32MP1 650MHZ 448LFBGA201 - Immediate$11.62Näytä tiedot
32-BIT ARM CORTEX-A7 900MHZ MPUSTM32MP135FAE732-BIT ARM CORTEX-A7 900MHZ MPU396 - Immediate$10.07Näytä tiedot
IC MPU STM32MP1 650MHZ 448LFBGASTM32MP153CAA3IC MPU STM32MP1 650MHZ 448LFBGA0 - Immediate$13.84Näytä tiedot