YAGEO
Tuotekategoriat

Digital Architecture Passive Components
Our interactive tool is here to guide you through each stage of a digital architecture system consisting of the input stage, the switch tank converter, the DC-DC converter, the digital processor, and finally all the inputs and outputs.

Power Conversion Passive Components
Our interactive tool is here to guide you through each stage of a power conversion system consisting of the EMI filter, the power factor corrector, the DC-DC converter, and finally the output filter.

TVS Circuit Protection
YAGEO's TVS have fast response speeds to protect sensitive electronic equipment from voltage transients induced by lightning and other transient voltage events.
Tools and Support
Tuoreet PTM:t
Tietoja yrityksestä YAGEO
Established in 1977, YAGEO has become a world-class provider of passive components services with capabilities on a global scale, including production and sales facilities in Asia, Europe and the Americas. The corporation provides one-stop-shopping, offering its complete product portfolio of resistors, capacitors and wireless components to meet the diverse requirements of customers. YAGEO currently ranks as the world No.1 in chip-resistors, No. 3 in MLCCs and No. 4 in ferrite products, with strong global presence - 21 sales offices, 9 production sites and 2 R&D centers worldwide. YAGEO’s product offerings are targeting at key vertical markets, including consumer electronics, computers & peripherals, industrial/power, alternative energy and automotive. They serve leading global customers, such as EMS, ODM, OEM and distributors.