YSAECLOUD1 Renesas Synergy™ Cloud Kit

Renesas' IoT development kit demonstrates Synergy Enterprise Cloud Toolbox application

Image of Renesas' YSAECLOUD1 Synergy™ Cloud KitThe YSAECLOUD1 Renesas Synergy Enterprise Cloud Toolbox from Renesas Electronics delivers practical examples of how to connect devices to any of three major enterprise cloud service providers in under 10 minutes. The Synergy platform’s powerful combination of security and connectivity solutions come together to make up a practical IoT application that developers can customize for their own end-applications. The Synergy Enterprise Cloud Toolbox is a Synergy Application Project available for download from renesassynergy.com providing step-by-step documentation and complete software projects to securely connect hardware using Synergy MCUs to any of three enterprise cloud service providers (Amazon Web Services, Google Cloud Platform™, or Microsoft Azure)in under 10 minutes. At no cost, developers can make this connection using a Renesas-hosted cloud account. They also can choose to integrate the connection with an existing cloud account. The Synergy Enterprise Cloud Toolbox enables users to visualize their sensor data on a private dashboard streaming live to the cloud from Synergy MCU-based hardware over Wi-Fi or a cellular connection. The full source for the dashboard is also included in the reference, further lowering the bar for developers to get started. The YSAECLOUD1 Cloud kit from Renesas accelerates design time, providing a faster time to market by connecting users embedded applications to the cloud quickly and easily.

Connection Diagram

Benefits

  • IoT developers must factor in time spent on cloud connectivity devices they manufacture, deploy, and maintain over the lifetime of the products
  • The Enterprise Cloud Toolbox takes care of several of the major challenges for developers of IoT application, without any need for complicated licensing schemes

Target Applications

  • Deployed, networked IoT devices that monitor and/or control surrounding environment and mechanisms - just about anything that has a MCU connected to the network
  • Home automation, industrial automation, building automation, and appliances

Kit Contents

  • MCU board
    • Renesas Synergy™ S5D9 MCU Group with Arm® Cortex®-M4F at 120 MHz with 2 MB Flash and 640 KB SRAM
    • The MCU board also offers 256 Mbits serial NOR QSPI Flash, 6-axis digital compass, microphone, barometric pressure, relative temperature and humidity sensors, 10/100 Base-T Ethernet port, USB 2.0 full speed (device and 5 V power), two grove connectors (I2C/GPIO, UART/GPIO), and three colored LEDs (red, yellow, and green)
  • Wi-Fi board
    • Offering 802.11 b/g/n connectivity using Qualcomm Atheros’ QCA4002, supported by the Synergy Wi-Fi framework
  • Debugger and cable
    • SEGGER J-Link® Lite for Renesas Synergy debugger and cable
  • USB cables
    • 2 x A male to Micro B male 1 ft. cables
  • Embedded software
    • Programming at the API level using Synergy Software Package (SSP) with production ready RTOS, middleware, security, frameworks, libraries, and drivers. Please visit the Renesas Synergy Gallery for more information and downloads, including professional grade development tools
  • Cloud services
    • Support for Renesas IoT Sandbox, a free prototyping environment including cloud-based developer accounts and editable mobile apps for iOS and Android. If users have not yet selected a cloud vendor but need to quickly build an IoT prototype, then the Renesas IoT Sandbox is a great way to get started
    • If the user already selected Amazon Web Services, Microsoft Azure, or Google Cloud Platform, then the Synergy Enterprise Cloud Toolbox application project and associated Renesas Cloud Dashboard can help them get connected to those cloud services with Synergy very quickly

YSAECLOUD1 Renesas Synergy Cloud Kit

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
SYNERGY S5 EVAL BRDYSAECLOUD1SYNERGY S5 EVAL BRD13 - Immediate$136.85Näytä tiedot
Published: 2018-02-27