Trion® T20 MIPI D-PHY/CSI-2 Development Kit

Efinix's Trion T20 MIPI D-PHY/CSI-2 camera prototyping platform helps users to quickly and easily prove project architecture and debug designs

Image of Efinix's T20 MIPI D-PHY/CSI-2 Development Kit Block Diagram Efinix® presents the Trion T20 MIPI D-PHY/CSI-2 development kit, a camera prototyping platform enabling interconnect to industry-standard camera/module solutions. The kit allows users to easily create a module based on their targeted vision sensor. The cost optimized, low power Trion T20 device used in this kit incorporates two fully enabled MIPI D-PHY/CSI-2 pre-engineered transmit/receive hard blocks. These Trion family members are ideal for applications that need to interface with the latest MIPI CSI-2 v1.3 camera sensors with enough programmable logic to handle image processing functions, merging/overlay, or analysis in a single device (manipulate, interpret, or analyze). With this board, users can quickly and easily prove their architecture and debug their design implementation. Applications include prototyping for machine vision, drones, robotics, surveillance, wide-field cameras (180/360), IoT, non-vision cameras, presence detection, consumer, and edge intelligence.

With the purchase of the Trion development kit, customers receive a single-seat license for the Efinity® software with one year of software maintenance, including updates and upgrades. The Efinity software provides a complete tool flow from RTL design to bitstream generation, including synthesis, place-and-route, and timing analysis. It has a graphical user interface (GUI) that provides a visual way to set up projects, run the tool flow, and view results. The software also has a command-line flow and Tcl command console. The software-generated bitstream file is used to configure the Trion FPGA on the development board with a custom design.

The purchase of this Trion development kit also includes access to the Efinix support center, which contains links to documentation, software, code examples, knowledgebase, and forum.

Features
  • T20 FPGA in a 169-ball BGA package
  • MIPI headers (2 TX and 2 RX)
  • 2 Raspberry PI camera connector daughter cards (camera, Raspberry Pi board interconnect, or both)
  • LVDS expansion daughter card
  • 2 user LEDs
  • 2 user pushbutton switches
  • Micro-USB port
  • SPI and JTAG headers to facilitate configuration
  • LVDS headers
  • GP headers that also connect with an SDRAM (B) board
  • 50 MHz and 74.25 MHz oscillators, optional SMA clock input
What Is Included
  • Trion T20 MIPI development board preloaded with MIPI demonstration design
  • Efinity software and one year of maintenance included for patches and upgrades
  • MIPI and LVDS expansion daughter card
  • 2 Raspberry PI camera connector daughter cards
  • Access to Efinix online support center for specialized access to design specific information
  • 15-pin FFC/FPC cable
  • Micro-USB cable
  • 10 standoffs
  • 6 nuts
  • 10 screws

Image of Efinix MIPI/CSI-2 Interop with Leopard Imaging  MIPI/CSI-2 Interop with Leopard imaging LI-IMX185-MIPI-M12 featuring Sony IMX185 sensor

Image of Efinix Trion T20 MIPI Development Board  MIPI/CSI-2 input switch example using Raspberry Pi camera module featuring Sony IMX219 sensor

Trion® T20 MIPI D-PHY/CSI-2 Development Kit

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
TRION T20 F169 EVAL BRDT20MIPI-DKTRION T20 F169 EVAL BRD88 - Immediate$127.49Näytä tiedot

ICs

KuvaManufacturer Part NumberKuvausToimintalämpötilaSaatavana oleva määrä HintaNäytä tiedot
IC FPGA 73 I/O 169FBGAT20F169C3IC FPGA 73 I/O 169FBGA0°C – 85°C (TJ)4115 - Immediate$9.03Näytä tiedot
IC FPGA 73 I/O 169FBGAT20F169I4IC FPGA 73 I/O 169FBGA-40°C – 100°C (TJ)1408 - Immediate$12.59Näytä tiedot

Leopard Imaging Camera and MIPI cable

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
MODULE CAMERA SONY/IMX185 MIPILI-IMX185-MIPI-M12MODULE CAMERA SONY/IMX185 MIPI40 - Immediate$211.63Näytä tiedot
MICRO COAX I-PEX CABLE: 300MMFAW-1233-03MICRO COAX I-PEX CABLE: 300MM0 - Immediate$29.75Näytä tiedot

Raspberry Pi Camera Module

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
RPI CAM V2 IMX219 8MPSC0023RPI CAM V2 IMX219 8MP0 - Immediate$12.75Näytä tiedot

Additional Components

KuvaManufacturer Part NumberKuvausSaatavana oleva määrä HintaNäytä tiedot
SBC 1.5GHZ 4 CORE 4GB PI 4 MOD BSC0194(9)SBC 1.5GHZ 4 CORE 4GB PI 4 MOD B9531 - Immediate$84.99Näytä tiedot
SBC 1.5GHZ 4 CORE 2GB PI 4 MOD BSC0193(11)SBC 1.5GHZ 4 CORE 2GB PI 4 MOD B0 - Immediate$46.74Näytä tiedot
Published: 2019-11-19