Webinar - Connectivity Solutions for Warehouse Automation

Connectivity is crucial in most facets of the supply chain. With the volume of goods needing to be shipped growing exponentially, the only way to keep up with demand is to increase the speed of each step in the process. The best way to achieve this is by adding more automation, which increases the need for reliable connectivity.

Thankfully, TE Connectivity and DigiKey are teaming up to discuss solutions that will help alleviate these challenges. Dr. Daniel König, Strategic Business Development Warehouse Automation & Robotics, and Dr. Jane Yun, Antenna Solutions Architect, have almost 30 years of combined experience in this field.

The webinar will be held on August 2nd, 2023, at 10 AM CDT. If you are unable to attend the live webinar, register to receive a recording when it has been completed.

Register here: https://event.on24.com/wcc/r/4270531/E627FF7341C7A7B322934FAFF921EED1?partnerref=blog

Tietoja kirjoittajasta

Image of Ashley Awalt

Ashley Awalt on teknisen sisällön kehittäjä ja hän on työskennellyt DigiKey Electronicsille vuodesta 2011 alkaen. Hän suoritti Associate of Applied Science -tutkinnon elektroniikkateknologiassa ja automatisoiduissa järjestelmissä Northlandin Community & Technical Collegessa Digi-Keyn apurahan avulla. Hänen nykyinen roolinsa on auttaa ainutlaatuisten teknisten projektien luomisessa ja niiden dokumentoinnissa sekä osallistuminen projektia käsittelevän videon tekemiseen. Vapaa-ajallaan Ashley mielellään – ei, hetki, onko äideillä lainkaan vapaa-aikaa?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum