Shorten Wireless Time-to-Market Development with Digi

When looking for a quicker-to-market alternative to chip-down design for networking operations, I found the new Digi IX15. It is versatile in that it can work as both an Digi XBee® gateway and a cellular router. The Digi IX15 is industrial-grade and can be used for building a cellular network with connectivity to the cloud or data centers. Because of the industrial nature of this device and its C1D2 certification, it will work great for applications such as oil and gas, wastewater, agriculture, and more. Using the Digi IX15 with Digi Remote Manager® allows the user to gain information, manage devices, and manage firmware updates. A few key features are dual SIMs for redundant connectivity, built-in Digi TrustFence® for security and privacy, ethernet and serial ports, edge compute programmability via Python, and much more.

Using the Digi IX15, Digi XBee 3 Zigbee Mesh Kit, Digi IX15 accessory kit, and Digi Remote Manager one-year subscription, a user can create a full cellular network system that works for many applications.

Tietoja kirjoittajasta

Image of Kelsie McMillin

Kelsie McMillin, Digi-Keyn strategisten ohjelmien kumppanuusmarkkinointipäällikkö, on työskennellyt yrityksessä vuodesta 2015. Hän työskentelee kaikkien IoT-teknologiaan liittyvien tuotteiden ja palveluiden parissa. Kelsie on suorittanut Associate of Applied Science -tutkinnon elektroniikkatekniikassa ja automatisoiduissa järjestelmissä Northland Community & Technical Collegessa DigiKey-stipendiohjelman kautta. Vapaa-ajallaan hän nauttii seikkailuista perheensä kanssa.

More posts by Kelsie McMillin
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum