ZFS Series Appl Sheet Datasheet by JKL Components Corp.

JK ® COMPONENTS CORPORATION 0 [IS lIS'I'ED S-CHO-BJ a. ZFS-CNL-aJ connectors with LED Hex m l.~ .+ JKU COMPONENTS CORPORATION
ZFS-CH0-8J & ZFS-CNL-8J connectors with LED flex
ZFS-CH140-I connector with LED flex
Since 1972
Q
u
a
l
i
t
y
L
i
g
h
t
i
n
g
S
o
l
u
t
i
o
n
s
800-421-7244
WWW.JKLLAMPS.COM
SALES@JKLLAMPS.COM
ZFS-SERIES
APPLICATION SHEET
LED Flex Ribbon - Compatible Dimmers & Controllers:
ZDM-01 LED Manual Dimmer
ZDM-02 LED Remote Control Dimmer
ZCTR-04 LED Photo Sensor Switch
ZCTR-08 LED Small Remote Controller
ZCTR-06 LED RGB Controller
ZCTR-05 LED Double-White Controller
ZCTR-07 LED Touch Panel Double-White Controller
Joiner Connectors:
ZFS-CH0-8J ZFS-CNL-8J
ZFS-CH138-8J ZFS-CNT-8J
ZFS-CH0-12J ZFS-CNX-8J
ZCH-137HD-8J
ZFS-CHBB-8J
ZFS-CHBB-10RGBJ
SELECT PRODUCTS
ROHS COMPLIANT
ISO9001 CERTIFIED
STANDARD INTENSITY (Economy)
SAMPLE
CONNECTORS
HIGH DENSITY (Tight Pitch)
HIGH INTENSITY
WATER RESISTANT
SIDEVIEW
ADJUSTABLE RGB COLOR
ADJUSTABLE WHITE
ZFS-CNT-8J
ZFS-CNX-8J
ZCH-170-RGB-J ZFS-CNL-8J
JK ® COMPONENTS CORPORATION SEE JKL’S APPLICA noN SHEET .IKL-AS-ZFS-DUAL-WHITE (7N TNIS 175M FOE ADDITIONAL DETAIL
Part Series
Wattage
Per Reel Reel Length Max Length
in Series Color Options
Connector
Options
Adjustable
Color RGB
SEE JKL'S APPLICATION SHEET JKL-AS-ZFS-DUAL-WHITE ON THIS ITEM FOR ADDITIONAL DETAIL
ZFS-SERIES
APPLICATION SHEET p. 2
1 METER = 3.25 FEET CW = Cool White, NW = Warm White, WW = Warm White
ZFS-8500 21.6 Watts 5 Meter 10 Meter
ZFS-CH140-8I - Input, 5” lead
ZFS-CH0-8J - Joiner, no lead
ZFS-CH138-8J - Joiner, 5” lead
ZFS-CNL-8J - “L” connection
ZFS-CNT-8J - “T” connection
ZFS-CNX-8J - “X” connection
Cool White (CW)
Neutral White (NW)
Warm White (WW)
Yellow
Standard
Intesity
Economy Flex
CW, NW, WW
Red
Blue
ZCH-143HD-8I - Input, 5” lead
ZFS-CHXB-8I - Input, no lead
ZCH-137HD-8J - Joiner, 5” lead
ZFS-CHBB-8J - Joiner, no lead
ZFS-85000HD 52.8 Watts 5 Meter 5 Meter
Max
Intesity
High Density
ZFS-85020WR 48 Watts 5 Meter 5 Meter CW, NW
Water resistant
ZFS-85000SV 24 Watts 5 Meter 5 Meter CW, NW
Sideview
ZFS-105000-DBW 25 Watts 5 Meter 20 Meter Adjustable White
Adjustable
White Output
ZFS-10504-RGB 36 Watts 5 Meter 5 Meter Adjustable RGB
ZFS-155000 57 Watts 5 Meter 5 Meter CW
SEE JKL'S APPLICATION SHEET JKL-AS-ZFS-RGB-LED ON THIS ITEM FOR ADDITIONAL DETAIL
Double LED
ZFS-84000 34.6 Watts 4 Meter 8 Meter CW, NW, WW
High Density
8mm width
ZFS-124000 46 Watts 4 Meter 8 Meter CW, NW, WW
High Density
12mm width
ZFS-125000HD 48 Watts 5 Meter 8 Meter Blue, Green
High Lumen
12mm width
ZFS-245000 67 Watts 5 Meter 8 Meter CW, NW, WW
High Lumen
10mm width
ZFS-104000 46 Watts 4 Meter 8 Meter CW, NW, WW
ZFS-105000-24RGB 72 Watts 5 Meter 5 Meter Adjustable RGB
High Lumen
10mm width
Adjustable
Color RGB
Adjustable
Color RGB ZCH-170-RGB-J - Joiner, 6” lead
ZCH-CH0-RGB10J - Joiner, no lead
ZFS-CH144-12I - Input, 5” lead
ZFS-CH0-12J - Joiner, no lead
Part Series
Feature
Feature Wattage
Per Reel
Reel Length
Reel
Length
Max Length
in Series
Color
Options Connector Options
LED FLEX RIBBON - 12VDC
LED FLEX RIBBON - 24VDC
ZCH-143HD-8I - Input, 5” lead
ZCH-137HD-8J - Joiner, 5” lead
Wattage
Per Reel
Max Length
in Series
Color
Options Connector Options
ZFS-CH144-12I - Input, 5” lead
ZFS-CH0-12J - Joiner, no lead
ZFS-CH144-12I - Input, 5” lead
ZFS-CH0-12J - Joiner, no lead
ZCH-170-RGB-J - Joiner, 6” lead
ZCH-CH0-RGB10J - Joiner, no lead
SEE JKL'S APPLICATION SHEET JKL-AS-ZFS-RGB-LED ON THIS ITEM FOR ADDITIONAL DETAIL
JK GCOMPONENTS CORPORATION
ZFS- SERIES
APPLICATION SHEET p.3
Once the type of flex ribbon has been selected and the total amount determined then the power
supply size can be established. This is determined by adding up all the number of reels of the flex
ribbon and any partial reels used. The chart on page 2 gives information on the amount of power
consumed by one reel of each style of LED Flex Ribbon. Multiply the number of reels & partial
reels by the power for one reel together to establish the power required.Power supplies should
have a rating of 15-20% more than the specifed wattage for safe, cool operation.
POWER INPUT
If a high wattage power supply is used, you can parallel connect LED lines, taking care not to
exceed the maximum series length indicated in the flex ribbon chart on page 2.
Optimum dimming is accomplished with a Pulse Width Modulating (PWM) dimmer, spuch as the
ZDM-01, which will maintain operating voltage to the ZRS ribbon. The dimmer varies the
duty-cycle to the LED which permits easy changes to the light output. The LED Ribbons can also
be set to turn on and off using other compatible devices such as JKL’s ZCTR-04 Photo Sensor
Switch which responds to ambient light.
OUTPUT
DIMMING
“STAR” Pattern Layout
POWER IN
LED RIBBON LED RIBBON
POWER
SUPPLY
LED RIBBON
The ZFS LED flex ribbon has adhesive backing and a paper cover strip that can be peeled away
for mounting to hard surfaces. Insulated staples can also be used to mount the LED flex ribbon
with care. If one LED is damaged, the segment may not light but the rest of the ribbon will light,
unless the main trace is damaged. If this is the case, the damaged section can be cut out and the
two pieces joined together using one of the joiner connectors.
All of the flex ribbons are made up of segments containing LEDs and a current controlling element.
Marks at the beginning and end of each segment indicate where the ribbon can be cut. The flex
ribbon can be cut with a pair of scissors or wire cutters at the marks. Input cables and joiner cables
can then be used to apply power, turn corners, change directions or create gaps with a jumper
where no light is desired. See chart for the appropriate segment lengths, cables and connectors.
The maximum recommended continuous length of flex ribbon is listed by part number iand
considers the current carrying capacity of the specific LED flex. In addition to the heat generated
by the LEDs (which must be dissipated via conduction through the flex ribbon), the flex ribbons
with higher current levels will generate added heat, which can affect the lumen output. If one
extends beyond the recommended length limit the voltage will be reduced, causing reduced
brightness.
INSTALLATION