114991496 Datasheet by Seeed Technology Co., Ltd

«bseeed Grove Universal 4 Pin to Beaglebone Blue 6 Pin Female lST/SH Conversion world. Previously we have developed the Grove cape for Beaglebone Series, it makes most different kind of modules such as sensors, displays, actuactors etc. However which makes it not possible using the Grove cape to connect Grove modules. That's why we Conversion Cable (10 pcs pack). ADC, on one side is the Grove Universal 4 Pin connector, on the other side is Beaglebone pin Conversion Cable, please clcik here to buy.
GroveUniversal4PintoBeaglebone
Blue6PinFemaleJST/SHConversion
Cable(10pcspack)
SKU114991496
Description
TheBeagleboneseriesareoneofthemostfamousopensourcedevelopmentboardinthe
world.PreviouslywehavedevelopedtheGrovecapeforBeagleboneSeries,itmakesmost
BeagleboneboardreachabletothegreatGrovesystemwhichincludesmorethan150+
differentkindofmodulessuchassensors,displays,actuactorsetc.However
theBeagleboneBluehasverydifferentlayoutfrommostoftheotherBeagleboneboard,
whichmakesitnotpossibleusingtheGrovecapetoconnectGrovemodules.That'swhywe
makethiscable‐GroveUniversal4PintoBeagleboneBlue6PinFemaleJST/SH
ConversionCable(10pcspack).
ItisaconversioncablespeciallymakeforusingGrovewithBeagleboneBlueviaGPIOand
ADC,ononesideistheGroveUniversal4Pinconnector,ontheothersideisBeaglebone
Blue6pinJST/SHconnector.WealsoprovideGroveUniversal4PintoBeaglebonBlue4
pinConversionCable,pleaseclcikheretobuy.
\\ x
TechnicalDetails
Weight G.W30g
BatteryExclude
PartList
GroveUniversal4PintoBeagleboneBlue6PinFemaleJST/SHConversionCable(10pcspack) 10
https://www.seeedstudio.com/GroveUniversal4PintoBeagleboneBlue6PinFemaleJST%2FSHConversionCable%2810pcspack%29p3027.html31218